Store_Parameters (Save Parameters)
| Index.Sub | 1010.1H | ||||||
| Data Type | Unsigned32 | ||||||
| Access | Read/Write | ||||||
| PDO Mappable | No | ||||||
| Unit | -- | ||||||
|
Range |
|
||||||
| Default Value | -- | ||||||
| Store Supported | -- | ||||||
| Description |
This object supports the saving of drive parameters in non-volatile memory. On reception of the correct signature the drive stores the current parameters values in non-volatile memory. At the next drive switch on the parameters starting value will be equal to the value stored in non-volatile memory. |
||||||
|
Notes |
The storing process takes about 4-5 (worst case) seconds to be completed. If a further store parameters command is sent before the completion of the previous one, the drive will not answer to the communication interface until the previous storing process is completed. The non-volatile ram is really written only if data have changed compared to the previous store process.
|